Use the System security settings tab to increase the security.
Property |
Description |
Enable external websites to be embedded into WebStation |
Select if you want external content to be embedded in WebStation. Enabling external websites to be embedded into WebStation lowers the security significantly. Do not enable external websites to be embedded into WebStation if you do not understand the security implications. |
Lists external websites that are allowed to be embedded into WebStation |
Type a list of websites that are allowed to be embedded into WebStation. The list is a white list of allowed external websites. Enabling external websites to be embedded into WebStation lowers the security significantly. Do not enable external websites to be embedded into WebStation if you do not understand the security implications. |
Enable WebStation to be embedded into another site |
Select if you want WebStation to be embedded in another web site. |
Website to allow access to WebStation when embedded |
Type a list of websites that are allowed to access WebStation when WebStation is embedded in the website. |
Enable WebStation to use unsafe string evaluated JavaScript methods |
Select if you have graphics written in older versions of EBO that cannot be displayed in 3.0 or later. |
Enable HSTS pre-load list |
HSTS is a preload list supported by Google. It requires a valid certificate on the server. Refer to Google HSTS documentation for more information. |
HSTS pre-load list max-age |
HSTS is a preload list supported by Google. It requires a valid certificate on the server. Refer to Google HSTS documentation for more information. |