SmartX Servers

1048 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Information Type
Topic
Modified
Rating
Setting the Time Increments in the Server Time Bar
You set the time increments in the Server Time bar to adjust the time value bars in the Graphic View.
3/4/2019
Delete Object Dialog Box
The Delete object dialog box is displayed when you try to delete an object you are not allowed to delete.
2/27/2019
2/21/2019
Creating an Alarm Triggered Notification
You configure an alarm triggered notification to notify users when an alarm condition is met.
1/23/2019
Wiring a Terminal Base
You can wire a terminal base prior to installing an electronics module.
1/11/2019
Output Override Function
The output override function allows you to manually override outputs. This function can be used for testing, commissioning, and maintenance of equipment.
12/20/2018
Configure Inputs and Outputs for Temporary Use
In configuration mode, you can locally configure inputs and outputs for temporary use during commissioning of the device. You can configure inputs and outputs that have not been configured through WorkStation.
12/20/2018
Trend Log List Context Menu
Right-click a row in a trend log list to open the trend log list context menu, where you can edit a record, show the history of a record, or copy the trend log list data.
12/20/2018
Acknowledged Style Properties
Use the Acknowledged Style properties to edit and view the colors and fonts of alarms in Alarms pane and Alarm Views that are in acknowledged state.
12/11/2018
Communication Port Wiring
The wiring recommendations for the SmartStruxure server device communication ports apply to the wires and cables used for RS-485 communications, LonWorks communications, USB connections, and Ethernet connections. Always use the recommended cables and wires.
12/6/2018

Product version

Language