WorkStation

413 Topic(s)
Use the filters below to limit the number of search hits.
Functionality
Information Type
Topic
Modified
Rating
Interval Trend Logs
​The interval trend log collects data at a specific time interval. Each logged value is stored as a record in the trend log. Use this trend log when the logging interval is less than 1 hour.
3/13/2019
Creating an Interval Trend Log
You create an interval trend log to record a value of a variable at specified and regularly occurring increments of time.
3/8/2019
Editing the Grid Time Interval
You edit the grid time interval for the shedule view to define how precis you can be when editing the time span of a schedule event using the drag and drop method.
3/4/2019
1/22/2019
User Menu – Measurement System Submenu
Use the Measurement submenu to choose the measurement system for your Workstation.
1/9/2019
How Alarms Work
You are notified by alarms when some important event occurs. For example, if the temperature is too low or too high in a building, if a window is open, or if something is broken, such as a fan. The system administrator sets up the alarms and decides to whom the alarm is sent.
1/2/2019
Weekly Events in WorkStation
A weekly event occurs every week for an extended period of time on a regular basis. You can schedule more than one weekly event for each day of the week.
12/20/2018
Trend Log Lists in WorkStation
A trend log list displays all values in the trend log in a list.
12/20/2018
Showing Trend Chart Grid Lines
You show the trend chart grid lines on the x-axis and the y-axis to make the chart easier to read.
12/20/2018
Showing Markers in a Trend Log Series
You show trend log series with markers for each record to make reading easier.
12/19/2018

Product version

Language