The License Information bar displays the status of the licenses. It displays if licenses are missing or if a license has expired or is about to expire. The bar also informs you if you are running on Demo or Engineer licenses. For more information, see License Enforcement .
Component |
Description |
Licensing Information |
Click to open License Manager to get more information regarding required licenses. |
Hide |
Click Hide to hide the License Information bar for a per-defined time frame. After 30 days, the bar turns red. |