earth_america
user_standard Iniciar sesión
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Interfaz de usuario

Interfaz de usuario


Productos Enterprise Central, Enterprise Server, Software Administrator
Funcionalidades: Ingeniería
Versión del producto: 2.0, 2.1, 3.0, 3.1
18/07/2025

Software Administrator – Enterprise Central View

Use the Enterprise Central view ​to start and stop the Enterprise Central service and configure the ports of Enterprise Central.

 
action_zoom_plus_stroke Enterprise Central view
Figura: Enterprise Central view

Tabla: Enterprise Central View

Component

Description

Status

Displays the current status of the Enterprise Central Windows service.

Start Service

Click to start Enterprise Central.

Stop Service

Click to stop Enterprise Central.

HTTP Port

Type the port number that Enterprise Central listens to when communicating through the Hypertext Transfer Protocol.

HTTPS Port

Type the port number that Enterprise Central listens to when communicating through the Hypertext Transfer Protocol Secure.

TCP Port

Type the port number that Enterprise Central listens to when communicating through the Transmitting Control Protocol.

System

Displays the system log.

Path

Displays the path to the folder where the Enterprise Central database and other objects created by Enterprise Central or users are stored.

 
action_zoom_plus_stroke

A warning indicates that you entered a conflicting port number or that the service is stopping.

  • Starting the Enterprise Central Windows Service
  • Stopping the Enterprise Server Windows Service
  • Restarting the Enterprise Server Windows Service
  • Software Administrator
  • ​Configuring Server Port Settings