earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-P-3, AS-B, Edge Server, Device Administrator, AS-P
Functionalities: Engineering, License Management
Product version: 7.0
9/30/2025

Assign and Activate Licenses

arrow1_rotationAssign Licenses arrow1_rotationActivate Licenses

When you have added the Entitlement to Device Administrator, you must assign and then activate the licenses on the EcoStruxure BMS servers.

Assign Licenses

Assigning licenses is the process of distributing the licenses from the Entitlement to the EcoStruxure BMS servers in the list.

Activate Licenses

When you have assigned the licenses to the EcoStruxure BMS servers, you must activate the licenses. Activation is required for enabling features that require licenses. Activation is done on the EcoStruxure BMS server level. You can activate licenses for all EcoStruxure BMS servers in the list at the same time. Or you can choose to select a subset of servers and activate licenses for just those servers.

Online activation

Online activation is implemented immediately. Online activation requires that the EcoStruxure BMS servers or the computer that runs Device Administrator is connected to the Internet.

For more information, see Activating Licenses Online .

Online activation on a semi online system

A special case is semi online system where the EcoStruxure BMS server is not connected to Internet, but Devices Administrator is connected to Internet.

In this case, Device Administrator acts as a bridge between the offline EcoStruxure BMS server and License Activation Server.

For more information, see Semi Online System .

For more information, see Activating Licenses Online .

Offline activation

Offline activation is used when the EcoStruxure BMS server does not have any access to the internet. Offline activation is a multi-step process.

After the licenses are assigned, you create a set of request files using Device Administrator. The request files are then uploaded to the FlexNet Operations Administrator server. The FlexNet Operations administrator server processes the request files and creates a set of response files. The response files are downloaded and copied to the computer that runs Device Administrator. The response files are sent from Device Administrator to the EcoStruxure BMS server.

For more information, see EcoStruxure BMS Server Licensing on Servers not Connected to Internet Workflow .

  • Centralized Licensing Overview
  • EcoStruxure BMS Server Licensing on Servers not Connected to Internet Workflow
  • Centralized Licensing on EcoStruxure BMS Servers Connected to Internet Workflow
  • Activating Licenses Online
  • Assigning Licenses
  • Semi Online System