earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: AD v3
功能: 硬件
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
2024/10/7

AD v3 Safety Information

arrow1_rotationCleaning AD v3

This section provides safety information specific to AD v3. Carefully read the instructions before trying to install, operate, service, or maintain the equipment.

The AD v3 specific safety instructions below is used with the standard safety information. 有关更多信息,请参阅 安全信息 .

Never open the equipment. For safety reasons, the equipment should be opened only by qualified service personnel. If one of the following situations arises, get the equipment checked by service personnel:

  • The power cord or plug is damaged.

  • Liquid has penetrated into the equipment.

  • The equipment has been exposed to moisture.

  • The equipment does not work well, or you cannot get it to work according to the user documentation.

  • The equipment has been dropped and damaged.

  • The equipment has obvious signs of breakage.

重要:

Opening the equipment to make any changes or modifications to the equipment may invalidate all applicable regulatory and agency certifications and approvals.

Do not leave this equipment in an environment where the storage temperature may go below -20 °C (-4 °F) or above 60 °C (140 °F). This could damage the equipment. The equipment should be in a controlled environment.

通知

EQUIPMENT DAMAGE

Do not leave this equipment in an environment where the storage temperature may go below -20 °C (-4 °F) or above 60 °C (140 °F).

Failure to follow these instructions can result in equipment damage.

AD v3 contains a battery that provides power to the internal real-time clock (RTC). There is a risk of explosion if the battery is incorrectly replaced.

AD v3 contient une pile qui alimente l’horloge en temps réel interne. Il y a un risque d’explosion si la pile est remplacée incorrectement.

警告 警告

HAZARD OF EXPLOSION OR EQUIPMENT DAMAGE

  • Replace the battery only with same or equivalent battery type recommended by the manufacturer.

  • Discard used batteries according to the manufacturer's instructions.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

 
action_zoom_plus_stroke

Cleaning AD v3

通知

EQUIPMENT DAMAGE

  • Use a soft, pre-moistened lint-free cloth for cleaning.

  • Avoid getting moisture in openings.

  • Do not spray anything directly on the equipment.

  • Do not use compressed air.

  • Do not use caustic or corrosive products, ammonia, solvents, or any cleaning product containing alcohol or grit.

Failure to follow these instructions can result in equipment damage.

  • Hardware Overview
  • AD v3
  • 安全信息