The RP controller expansion blind modules enable control of motorized window blinds and shutters.
The blind modules support blind motors that operate on AC mains voltage (230 VAC) as well as DC motors (24 VDC). The blind modules also come in different models that support blind motor drives with Standard Motor Interface (SMI) as well as conventional motor drives.
Module |
Blind Motor |
SMI-interface |
RP-C-EXT-BL-SMI-4-HV-PD |
230 VAC |
yes |
RP-C-EXT-BL-SMI-2-LV-PD |
24 VDC |
yes |
RP-C-EXT-BL-4-HV-PD |
230 VAC |
no |
RP-C-EXT-BL-2-LV-PD |
24 VDC |
no |
The RP-C-EXT-BL-SMI-4-HV-PD SMI blind module connects to the RP controllers and provides I/O expansion for control of AC mains-supplied motors (drives) with SMI (Standard Motor Interface for AC applications).
For more information, see RP-C-EXT-BL-SMI-4-HV-PD .
The RP-C-EXT-BL-SMI-2-LV-PD SMI blind module connects to the RP controllers and provides I/O expansion for control of DC low-voltage motors (drives) with SMI LoVo (Standard Motor Interface for low-voltage applications).
For more information, see RP-C-EXT-BL-SMI-2-LV-PD .
The RP-C-EXT-BL-4-HV-PD blind module connects to the RP controllers and provides I/O expansion for high-voltage blind control.
For more information, see RP-C-EXT-BL-4-HV-PD .
The RP-C-EXT-BL-2-LV-PD blind module connects to the RP controllers and provides I/O expansion for low-voltage blind control.
For more information, see RP-C-EXT-BL-2-LV-PD .