earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-P-3, AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Security
Product version: 7.0, 7.1
11/5/2025

System Security Settings Tab

Use the System security settings tab to increase the security.

 
action_zoom_plus_stroke System security settings tab
Figure: System security settings tab

Property

Description

Enable external websites to be embedded into WebStation

Select if you want external content to be embedded in WebStation.

Enabling external websites to be embedded into WebStation lowers the security significantly. Do not enable external websites to be embedded into WebStation if you do not understand the security implications. For more information, see HTML Utilities .

Lists external websites that are allowed to be embedded into WebStation

Type a list of websites that are allowed to be embedded into WebStation. The list is a white list of allowed external websites.

Enabling external websites to be embedded into WebStation lowers the security significantly. Do not enable external websites to be embedded into WebStation if you do not understand the security implications. For more information, see HTML Utilities .

Enable WebStation to be embedded into another site

Select if you want WebStation to be embedded in another web site. For more information, see Security Configuration in WebStation .

Website to allow access to WebStation when embedded

Type a list of websites that are allowed to access WebStation when WebStation is embedded in the website.

Enable WebStation to use unsafe string evaluated JavaScript methods

Select if you have graphics written in older versions of EBO that cannot be displayed in 3.0 or later. For more information, see Cannot Open Graphics in WebStation .

Enable HSTS pre-load list

HSTS is a preload list supported by Google. It requires a valid certificate on the server. Refer to Google HSTS documentation for more information.

HSTS pre-load list max-age

HSTS is a preload list supported by Google. It requires a valid certificate on the server. Refer to Google HSTS documentation for more information.

Content Security Policy Report Uri

If Content Security Policy (CSP) is used, type the address to CSP report server.

For more information, see Content Security Policy Report Uri .

  • Security Configuration in WebStation
  • Settings Menu – Options Tab
  • Cannot Open Graphics in WebStation