Log on to rate and give feedback    1 2 3 4 5 Log on to rate
0
Concept Concept 1/24/2022
Products: Function Block Editor
Functionalities: Programming
Product version: 2022

Blocks and Operators Lists in Builder for Function Block

The list of blocks, operators and expression blocks available for Function Block programming in Library of Builder Edit Mode.

For more information, see Simple Blocks .

Blocks List

Function Block Programs

Connections

BI

For more information, see BI – Binary Input .

BO

For more information, see BO – Binary Output .

RBO

For more information, see RBO – Relinquish Binary Output .

II

For more information, see II – Integer Input .

IO

For more information, see IO – Integer Output .

RIO

For more information, see RIO – Relinquish Integer Output .

PI

For more information, see PI – Pulse-Counter Binary Input .

PO

For more information, see PO – Pulsed Binary Output .

RI

For more information, see RI – Real Input .

RO

For more information, see RO – Real Output .

RRO

For more information, see RRO – Relinquish Real Output .

Signal Sources

NCYC

For more information, see NCYC – Program Cycle Counter .

OSC

For more information, see OSC – Oscillator .

PVB

For more information, see PVB – Parameter Value Binary .

PVI

For more information, see PVI – Integer Value Parameter .

PVR

For more information, see PVR – Real Value Parameter .

Logical Functions

AND-AND gate

For more information, see AND – Logical AND Gate .

NOT-NOT gate

For more information, see NOT – NOT Gate .

OR-OR gate

For more information, see OR – OR Gate .

PULSE

For more information, see PULSE – Pulse Generator .

SR

For more information, see SR – Set-Reset Flip-Flop .

TRIG

For more information, see TRIG – Trigger .

XOR

For more information, see XOR – Exclusive OR Gate .

Non-linear Functions

AHYST

For more information, see AHYST – Analog Hysteresis .

HYST

For more information, see HYST – Binary Hysteresis .

LIMIT

For more information, see LIMIT – High/Low Signal Limit .

MAX

For more information, see MAX – Maximum Signal Selector .

MIN

For more information, see MIN – Minimum Signal Selector .

Delays

DELAY

For more information, see DELAY – Delayed On/Off .

DELB

For more information, see DELB – Binary Value Delay .

DELI

For more information, see DELI – Integer Value Delay .

DELR

For more information, see DELR – Real Value Delay .

SHB

For more information, see SHB – Sample and Hold Binary Value .

SHI

For more information, see SHI – Sample and Hold Integer Value .

SHR

For more information, see SHR – Sample and Hold Real Value .

Controllers and Filters

FILT

For more information, see FILT – First Order Filter .

OPT

For more information, see OPT – Optimization .

PIDA

For more information, see PIDA – PID Controller – Analog Output .

PIDI

For more information, see PIDI – PID Controller – Incremental Output .

PIDP

For more information, see PIDP – PID Controller – Analog Output .

RAMP

For more information, see RAMP – Ramp Filter .

SEQ

For more information, see SEQ – Sequencer .

Accumulators

ACCUM

For more information, see ACCUM – Accumulator .

INTEG

For more information, see INTEG – Integrator .

RT

For more information, see RT – Run-Time Measurement .

System Variables

DATE

For more information, see DATE – Day .

ERROR

For more information, see ERROR – System Error .

HOUR

For more information, see HOUR – Hour .

MINUTE

For more information, see MINUTE – Minute .

MONTH

For more information, see MONTH – Month .

RST

For more information, see RST – Restart .

SECOND

For more information, see SECOND – Second .

TCYC

For more information, see TCYC – Cycle Time .

WDAY

For more information, see WDAY – Week Day .

Time Schedules and Alarms

ALARM

For more information, see ALARM – Alarm .

TSCHI

For more information, see TSCHI – Time Schedule .

Transformation Functions

CURVE

For more information, see CURVE – Curve Function .

ENTH

For more information, see ENTH – Enthalpy .

POLY

For more information, see POLY – Polynomial Function .

PRCNT

For more information, see PRCNT – Percentage .

VECTOR

For more information, see VECTOR – Vectorial Curve Function .

Expressions

For more information, see Expression Blocks .

XPB

Binary Expression

XPI

Integer Expression

XPR

Real Expression

Operators List

Operators

Constants

For more information, see Constant Operators .

Binary const

Integer const

Real const

Logicals

For more information, see Logical Operators .

NOT

AND

OR

XOR

Maths

For more information, see Math Operators .

Negate

Addition

Subtraction

Product

Division

Module

Comparisons

For more information, see Comparison Operators .

Less then

Greater than

Equal

Not equal

Greater or equal

Less or Equal

Bit

For more information, see Bit Operators .

bit AND

bit OR

bit XOR

Shift left

Shift right

Others

For more information, see Miscellaneous Operators .

A/D converter

D/A converter

Analog mux.

Digital mux.

Conversion AA

Community Content

Product version

Language