Log on to rate and give feedback    1 2 3 4 5 Log on to rate
0
Concept Concept 1/12/2022
Products: Function Block Editor
Functionalities: Programming
Product version: 2022

RIO – Relinquish Integer Output

The RIO block is an integer output from ​a function block program that can send out a value or null.

The relinquish integer output

The relinquish integer output

Note:

The RIO block has no parameters.

The RIO Block Input

Input

Data Type

Description

V

INTEGER

Input signal to send outside the program.

r

BINARY

Relinquish trigger. If TRUE, the output will be “null” and if FALSE the output is the same as the "V" value.

The RIO Block Output

Data Type

Access

INTEGER

RO

Community Content

Product version

Language