earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: (None)
Functionalities: Engineering
Product version: 2024, 7.0
3/20/2025

Clean Contact Output Properties – Basic Tab

Use the Basic​ tab to view and update basic properties of the clean contact output.

 
action_zoom_plus_stroke Clean contact output properties – Basic tab
Figure: Clean contact output properties – Basic tab

Table: Clean contact output properties – Basic tab

Property

Description

IO function

Displays the IO function.

Contact description

Displays the contact description.

Index

Displays the index, which is a unique number set by the fire detection system.

  • General Information Properties – Basic Tab