earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Twisted Pair Adapter
Functionalities: Hardware
Product version: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0, 7.1
1/7/2026

Restarting the Twisted Pair Adapter

You restart the Twisted Pair Adapter to intialize the device.

Show More
action_close

The Twisted Pair Adapter has two controls on the front:

  • Push-button labeled “INIT”

  • 2-pole slide switch with positions labeled “M” and “T”

 
action_zoom_plus_stroke Push-button and slide switch
Figure: Push-button and slide switch
Push-button

The INIT push-button is used to reboot the Twisted Pair Adapter. Pressing this button for 2 seconds will restart the device without disconnecting it from power. For more information, see Restarting the Twisted Pair Adapter .

Slide switch

The slide switch is used to select the adapter’s operating mode:

  • M (Master) – Use this mode when the adapter is connected to an automation server. Only one adapter can operate as Master in a network.

  • T (Terminal) – Use this mode when the adapter is connected to a SpaceLogic BACnet/IP controller.

Switching between these positions configures the adapter for the appropriate network setup. For more information, see Changing the Twisted Pair Adapter Operating Mode .

To restart the Twisted Pair Adapter
  • Press the INIT push-button on the adapter front for 2 seconds.

     
    action_zoom_plus_stroke

When the adapter is initializing, all three LEDs on the front flash green synchronously. When the flashing stops, the device has finished initializing and has restarted itself. For more information, see Twisted Pair Adapter LEDs .

  • Twisted Pair Adapter
  • Twisted Pair Adapter Button and Switch
  • Twisted Pair Adapter LEDs