earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: Twisted Pair Adapter
Functionalities: Hardware
Product version: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0, 7.1
12/18/2025

Wire Sizes and Lengths for the Twisted Pair Adapter

This section outlines the recommended cables and wires, specifying the appropriate wire sizes and lengths for the Twisted Pair Adapter.

The recommendations are for guidance only. Other wire sizes and lengths may be used, depending on wiring rules and when appropriate.

Table: Wire Sizes and Lengths for the Twisted Pair Adapter

Terminals

Minimum Cross-sectional Area

Maximum Cable Length

Power input terminals (1, 2)

0.2 mm² (24 AWG) a

According to local wiring rules

Functional earth ground terminals (3, 4)

0.2 mm² (24 AWG) a b

According to local wiring rules

Twisted pair cable network (NET) terminals (5, 6)

0.52 mm² (20 AWG)

1200 m (3900 ft)
  1. Use wires rated for at least 90 °C (194 °F).
  2. The functional earth ground conductor must have a cross-sectional area at least equal to that of the power supply conductor.
  • Wire Sizes and Lengths
  • Twisted Pair Adapter
  • Twisted Pair Adapter Screw Terminals and Port
  • Wiring
  • Communication Port Wiring