You wire the screw terminals on a Twisted Pair Adapter to connect the adapter to a twisted pair cable network. Always use the recommended wires (or wires with larger cross-sectional area).
Loosen the screws of the terminals for network connection. For more information, see Twisted Pair Adapter Screw Terminals and Port .
Strip approximately 7 mm (0.3 inch) of the insulation from the end of each wire.
Insert the end of the wire fully into its intended terminals. Ensure that no bare wire strands extend from the terminal.
Tighten the screw using a small flat-blade screwdriver. Ensure that the screw is fully tightened. Use the following recommended screw tightening torque: 0.56 Nm (5 lbf.in).
Repeat steps 2 to 5 until all screw terminals for the network connection on the adapter are correctly wired. For more information, see Twisted Pair Adapter Screw Terminals and Port .
Terminals 5 and 6 are polarity insensitive.
Use appropriate cable strain relief methods, to help prevent any load applied to the cable from being transferred to conductor terminations.