earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-P-3, Enterprise Central, Enterprise Server, ​License Administrator, AS-P
Functionalities: License Management
Product version: 7.0, 7.1
12/18/2025

Centralized Licensing Connected Devices

Connected devices are devices connected to a field bus driven by an Enterprise server or automation server. The number of Connected Devices in a system is counted in order to establish the license quantity required for the system. The counting rules have remained unchanged since EBO 2022.

In general, all devices defined in the EBO system tree are counted. This includes devices connected behind a transparent gateway.

For example, devices behind Modbus IP gateways such as Panel Server and IFE, Zigbee devices behind a SE8000 are counted because they are transparently exposed to EBO. The exception to this rule is devices connected behind a MP or RP, they are accessible to EBO, however they are excluded from the device count.

Devices Defined as Connected Devices and Counted

Connected devices are devices that are directly connected to an Enterprise Server or an automation server AS-P, AS-B and AS-P-3 using standard protocol such as BACnet or Modbus.

In general, all devices defined in the EBO system tree are counted, except those defined under MP or RP.

Under the said conditions, the following devices are counted:

  • BACnet:

  • Infinity

  • Modbus

  • LonWorks

  • I/NET

  • NW8K

  • Infinet

  • Zigbee

  • 3rd party IO Modules

  • Sensors and actuators directly on a field bus are counted.

  • Transparent gateways.

Devices Not Counted

  • Automation servers.

  • SE Central IO modules 

  • LonWorks local nodes 

  • Devices connected to Space Logic Devices, for example RP/MP devices. 

Table: Examples

Scenario

Gateway Type

Count Gateway

Count Devices

Direct to AS/ES

N/A

N/A

Yes

PanelServer/IFE

Transparent

Yes

Yes

Modbus IP Gateway

Transparent

Yes

Yes

SE8000 Zigbee

Transparent passthrough

Yes (SE8000 itself)

Yes

MPC/RPC downstream

Controller exception

Yes (MPC/RPC)

No

  • Centralized Licensing Overview
  • Engineering Licenses Overview
  • Counting Connected Devices under a Field Server in old EBO System
  • Counting Connected Devices under an Enterprise Server using WorkStation