earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: AS-P-3, AS-B, Enterprise Central, Enterprise Server, AS-P
Functionalities: License Management
Product version: 7.0, 7.1
12/18/2025

Counting Connected Devices under an Enterprise Server using WorkStation

You count the required licenses so that you can order the correct amount on EcoStruxure Power and Buildings Software Companion. You use WorkStation to count licenses on devices under an Enterprise Server when upgrading from a system older than 6.0 to a 7.0 or higher.

To count connected devices using WorkStation
  1. In WorkStation, in the System Tree pane, select the top server.

  2. Click the Control Panel tab.

  3. Click Licenses Information .

  4. Click Licenses .

  5. The number of required licenses are displayed in the table.

  • Centralized Licensing Connected Devices
  • Engineering Licenses Overview
  • Counting Connected Devices under a Field Server in old EBO System