Click to rate and give feedback    1 2 3 4 5
User Interface User Interface 2/27/2019
Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Basic Functionality
Product version: 1.9

Delete Object Dialog Box

The Delete object dialog box is displayed when you try to delete an object you are not allowed to delete.

Delete object dialog box

Delete object dialog box

Delete Object Dialog Box

Command

Description

Apply to all selected objects

Select to apply the same command to all selected object(s).

Abort deletion

Click Abort deletion to keep all objects.

Ignore

Click Ignore to the delete the selected objects and keep objects that you are not allowed to delete.

Community Content

Product version

Language