earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: WebStation
Functionalities: Schedules
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0, 7.1
10/30/2025

Adding an Exception Event to a Xenta Schedule in WebStation

You add an exception event to configure an exception that is to apply instead of a scheduled weekly event for a single date, date range, or a time pair.

Show More
action_close

Xenta Time Schedules and Xenta Central Time Schedules can be edited in WebStation. You can add, edit and delete weekly and exception events. The Xenta Time Schedules and Xenta Central Time Schedules must be created using WorkStation.

For more information, see How Schedules Work .

Xenta Central schedules are used to group Xenta 280/300/401 LonWorks device schedules created in the TSCH block in Menta Editor. When you use a Central schedule, you can change settings on whole Xenta schedule groups from a central place.

For more information, see Xenta Central Schedules .

Important:

You cannot add, edit, or delete schedule events in a Xenta Schedule when a Xenta Central schedule has been assigned to it.

The number of events a Xenta Central schedule can have is determined by the Menta application.

Important:

An added exception event overrides any weekly events for all of the selected days.

To add an exception event to a Xenta Schedule in WebStation
  1. In WebStation, in the System Tree pane, select the schedule to which you want to add the exception event.

  2. In the Xenta Schedule editor, click Add .

  3. In the Interval type column, select Interval , On all day , or Off all day .

  4. If you select Interval in the Interval type column, enter the start time and end time for the interval.

  5. Select the weekdays the exception event is to be in service.

  6. Click Save .

  • Xenta Schedules in WebStation
  • Editing or Deleting a Weekly Event in a Xenta Schedule in WebStation