earth_america
user_standard 登录
action_search_stroke
earth_america
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
如何

如何


产品: Enterprise Central, Enterprise Server, Project Configuration Tool
功能: 本地化
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024
2024/11/29

Configuring Enterprise Server, Enterprise Central, and WorkStation Date and Time

You adjust the date and time of an Enterprise Server, Enterprise Central, or WorkStation through the operating system where Enterprise Server, Enterprise Central, or WorkStation is installed.

显示更多
action_close

​In WorkStation, all times are by default displayed in local time. This means that a time, independent of its source, is displayed in the same time zone as the operating system on which WorkStation is installed. By configuring the operating system time and time zone settings, you configure how times are displayed in WorkStation. For more information, please refer to the manufacturer’s manual for the operating system.

 
action_zoom_plus_stroke WorkStation displays all times as local time, according to the operating system settings on which WorkStation is installed.
图: WorkStation displays all times as local time, according to the operating system settings on which WorkStation is installed.

For example, a WorkStation in Athens surveys a SmartX server in New York. WorkStation in Athens has a Greek operating system, which is configured to Eastern European Summer Time (UTC +2h) with +1h DST offset. The New York SmartX server triggers an alarm at 07:43 Eastern time. WorkStation instantly reports the alarm but presents the alarm with the timestamp 14:43 which is the local time in Greece.

Some features in WorkStation, such as trend log and schedule, allow you to change the displayed time to UTC or server local time.

Server Time in WorkStation

The exception in WorkStation is the Local Date & Time property for the time on a SmartX server where the time is displayed in local server time and not in the perspective of WorkStation and its operating system.

To configure Enterprise Server, Enterprise Central, and WorkStation Date and Time
  1. Close all EcoStruxure Building Operation software applications.

  2. For more information on how to adjust the date and time, refer to the manufacturer’s manual for the operating system.

注释:

The time zone settings for an Enterprise Server and Enterprise Central are configured through WorkStation and not the operating system.

  • Changing the Time Zone of an EcoStruxure BMS Server
  • Creating a Custom Time Zone of an EcoStruxure BMS Server
  • Time and Time Zone Configuration in WorkStation
  • Time and Time Zone Configuration in Enterprise Server and Enterprise Central
  • Date & Time View
  • Enterprise Server does not Synchronize its Clock