earth_america
user_standard 登录
action_search_stroke
登录以评价并提供反馈 1 2 3 4 5 登录以评价
0
概念

概念


产品: WorkStation
功能: 基本功能
产品版本: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023
2024/12/5

用户体验

arrow1_rotation工作区 arrow1_rotation使用窗格的不同布局 arrow1_rotationWorkStation 快捷键 arrow1_rotation窗口

The Work area in the EcoStruxure BMS user interfaces may vary depending on how it is set up. A typical EcoStruxure BMS workspace contains panes and views.

工作区

The workspace in WorkStation and WebStation is the area where you perform all tasks at your site, such as acknowledging alarms and viewing trend logs.

有关更多信息,请参阅 工作区 .

使用窗格的不同布局

A pane is a separate area in the workspace. You use panes to carry out commands, navigate the system or display information. Panes can be moved, hidden, closed, and repositioned.

有关更多信息,请参阅 使用窗格的不同布局 .

WorkStation 快捷键

To ease the daily operation, you can use shortcut keys to most of the commands inWorkStation.

有关更多信息,请参阅 WorkStation 的键盘快捷方式 .

窗口

You can navigate between the available open windows in the Work area. The windows you can select using the Window menu are represented by tabs in the Work area.

有关更多信息,请参阅 窗口菜单 .

  • WorkStation 概览
  • 工作区
  • 使用窗格的不同布局
  • WorkStation 的键盘快捷方式
  • 窗口菜单