earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Schedules
Product version: 1.9
7/17/2020

Setting the Time Increments in the Server Time Bar

You set the time increments in the Server Time bar to adjust the time value bars in the Graphic View.

Show More
action_close

The Advanced view of the Schedule Editor has the features of the Basic view with some additional capabilities. All the tasks that you can perform in the Basic view, you can also perform in the Advanced view.

Unlike the Basic view, the Advanced view lists the exception and weekly events in an event tree. In addition, there is a Combined option that displays all the weekly and exception events for a selected date.

Two toggles provide additional options:

  • Mode : Switches between an editor or preview mode.

  • View : Switches between a graphical or text view.

 
action_zoom_plus_stroke Advanced view of the Schedule Editor
Figure: Advanced view of the Schedule Editor

Mode

The Mode toggle provides the following capabilities:

  • Editor mode where you can view or edit a weekly event or an exception event.

  • Preview mode where you can preview (but not edit) all the weekly schedules and exceptions for a selected date. However, only the effective weekly and exception events display for that date. Typically, you see one weekly and one exception event.

View

The View toggle provides the following capabilities:

 
action_zoom_plus_stroke Text View
Figure: Text View

Combined

You can view all of the events for a selected date using both the Combined option and Preview mode. Events can include exception and weekly events, and the Default value. You can toggle the combined events between the Graphic View or Text View .

 
action_zoom_plus_stroke Combined Events in Graphic View
Figure: Combined Events in Graphic View

For more information, see Advanced Schedule Editor Toolbar .

To set the time increments in the Server Time bar
  1. In WorkStation, in the System Tree pane, select the schedule you want to edit.

  2. In the Work area, click the Advanced tab.

  3. Click the Edit Schedule button

     
    action_zoom_plus_stroke
    .

  4. Click the Graphic View button

     
    action_zoom_plus_stroke
    .

  5. Right click on the Server Time bar, point to Snap To and select a time segment.

     
    action_zoom_plus_stroke
  6. Click the Save button

     
    action_zoom_plus_stroke
    .

You can modify a time value bar using the selected time increment. For more information, see Modifying a Time Value Bar in the Graphic View .

  • Advanced View of the Schedule Editor
  • Modifying a Time Value Bar in the Graphic View