You engineer your system using the engineering tools.
You use the Spreadsheet view to create and edit multiple objects and to save time.
For more information, see Spreadsheet Overview .
A binding is a connection between two or more variables for data exchange. In its simplest form, a binding consists of a source and a destination. The source supplies the value to the destination.
For more information, see Bindings Overview .
A text report provides a simple and quick method of obtaining a customized view of object property attributes.
For more information, see Text Reports Overview .
A solution or application is a user-created object or group of objects that perform a control process. Examples of creatable objects include networks, devices, programs, binding templates, graphics, trends, and alarms.
For more information, see Import and Export Overview .
Script programs are text-based instructions that tell the EcoStruxure BMS server to take some kind of action to control a building.
For more information, see Script Overview .
Function Block Editor is a graphical programming tool for EcoStruxure BMS servers and MP Series controllers, which you use to create function block programs that control and monitor building automation systems. For example, you create a basic program, called OfficeLight, to control lighting in a room based on occupancy.
For more information, see Function Block Editor Overview .
You can use Graphics Editor to create and edit graphics representing a site and the devices that make up the site.
For more information, see Graphics Editor .
WebReports is a Web application that you use to create, view, and administer reports. The reports provide information about alarms, trends, and user and system activity. You use the reports to help manage your building automation system.
For more information, see WebReports Overview .
Project Configuration Tool, with Project Configuration Tool client and WorkStation, is an offline engineering platform that is used for project configuration, virtual EcoStruxure BMS server configuration, and deployment. Project Configuration Tool supports the major communication protocols in the same way as other EcoStruxure Building Operation software products.
For more information, see Project Configuration Tool Overview .
To assess whether or not to convert a Vista system to an EcoStruxure BMS, you run an analysis of the Vista database export file to get information on the potential outcome of a conversion. The analysis is performed in TAC Vista Conversion Tool. If the analysis confirms that the Vista database is suitable for conversion, you can convert the database in TAC Vista Conversion Tool.
For more information, see Vista Conversion Overview .
Conversion is the process by which a customer's site is moved from Andover Continuum's legacy Building Management System to the EcoStruxure BMS. The Continuum Conversion Tool takes an ASCII dump from the Continuum system and creates EcoStruxure Building Operation objects that correspond to the objects in the ASCII dump file.
For more information, see Continuum Conversion Overview .
SmartX HMI Kiosk allows you to configure AD v3 as a dedicated HMI for local access to EcoStruxure BMS servers.
For more information, see SmartX HMI Kiosk Overview .