earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
How to

How to


Products: Automation Server, AS-B, Enterprise Server, AS-P, Project Configuration Tool
Functionalities: Alarms
Product version: 2.0, 2.1, 3.0, 3.1
2/22/2023

Adding an Attachment to Multiple Alarms

You add an attachment, for example a .pdf file or trend log, to assist the user when diagnosing or solving the problem that caused an alarm.

Note:

An alarm attachment is opened in a pop-up window only if the selected workspace contains the Alarm pane. For more information, see Workspace Components and Customization .

Show More
action_close

You can add attachments to alarm objects, except System Information alarms. An attachment is a link pointing to an object in the system. When an alarm that has an attachment is triggered, a paperclip icon is displayed in the Alarms pane and Alarm Views. It is also possible to configure the attachment to display when the alarm is going from Normal to Alarm state.

An attachment can be: a voice message, a report, a trend chart, a schedule, a Microsoft Word file, a PDF file, a video recording, or a pop-up window that contains information regarding the alarm.

You can add the same attachment or set of attachments to multiple alarms in a single operation. You can also delete the attachments that belong to multiple alarms in a single operation. If you add an attachment that already has been attached to an alarm, the later attachment is added as a duplicate.

You can open attachments provided that the program or editor associated with the attachment is locally installed on your computer. For example, if the attachment is a PDF file, you can open the file if Adobe Reader or a similar program is installed on your computer.

To add an attachment to multiple alarms
  1. In WorkStation, in the list view, select the alarms to which you want to add the alarm attachment.

  2. On the Actions menu, point to Advanced .

  3. Click Add attachment .

  4. In the Select Object dialog box, select the item that you want to attach to the alarms.

  5. Click Select .

  6. Click Yes if you want the attachment to display when the alarm is triggered.

  • Alarm Attachments
  • Workspace Components and Customization
  • Copying Attachments to Multiple Alarms
  • Removing Attachments from Multiple Alarms
  • Adding an Attachment to an Alarm
  • Removing an Attachment from an Alarm