earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AD v2, AD v1, AO-8, AO-V-8, Automation Server, AS-B, DI-16, DO-FA-12, DO-FC-8, MP-C, MP-V, AS-P, PS-24V, RTD-DI-16, UI-16, UI-8/AO-4, UI-8/AO-4 v2, UI-8/AO-V-4, UI-8/AO-V-4 v2, UI-8/DO-FC-4, UI-8/DO-FC-4 v2
Functionalities: Hardware
Product version: 2.0, 2.1
6/24/2026

Hardware Overview

arrow1_rotationTerminal Bases arrow1_rotationPS-24V Power Supplies arrow1_rotationAutomation Servers arrow1_rotationSmartX AS-P Servers arrow1_rotationI/O Modules arrow1_rotationSmartX AS-B Servers arrow1_rotationMP-Cs arrow1_rotationMP-Vs arrow1_rotationSmartX Sensors arrow1_rotationAD v1 arrow1_rotationAD v2 arrow1_rotationWiring

The Schneider Electric hardware devices for the EcoStruxure BMS include terminal bases, PS-24V power supplies, SmartX servers such as SmartX AS-P servers and SmartX AS-B servers, MP Series controllers such as MP-Cs and MP-Vs, I/O modules, and ADs.

Terminal Bases

The terminal bases are used for SmartX devices that are based on the patented two-piece design. The terminal base provides the I/O bus to the electronics module installed on the terminal base as well as to the SmartX device installed to the right (next terminal base in the chain).

For more information, see Terminal Bases .

PS-24V Power Supplies

PS-24V is the power supply for the SmartX AS-P servers, Automation Server, and I/O modules. The PS-24V power supply requires an input voltage of either 24 VAC +/–20 % or 24–30 VDC.

For more information, see PS-24V Power Supplies .

Automation Servers

An Automation Server is a Schneider Electric manufactured embedded device that generally serves as the lowest tier EcoStruxure BMS server within the EcoStruxure BMS. The Automation Server controls and supervises equipment, typically HVAC equipment. The Automation Server uses I/O modules with connected field devices, such as sensors and actuators, to do that.

For more information, see Automation Servers .

SmartX AS-P Servers

The SmartX AS-P server is the successor to Automation Server, and offers several improvements such as enhanced processor performance, increased memory size, dual Ethernet ports, and high-speed USB interfaces. Like the Automation Server, the SmartX AS-P server is a Schneider Electric manufactured embedded device that generally serves as the lowest tier EcoStruxure BMS server within the EcoStruxure BMS. The SmartX server controls and supervises equipment, typically HVAC equipment. SmartX AS-P servers use I/O modules with connected field devices, such as sensors and actuators, to do that.

For more information, see SmartX AS-P Servers .

I/O Modules

By adding a variety of I/O and power supply modules, you can use the SmartX AS-P server or Automation Server to tailor the Intelligent Building Management System to your unique requirements.

For more information, see I/O Modules .

SmartX AS-B Servers

A SmartX AS-B server is a powerful SmartX server that features both onboard I/O and built-in power supply. Like the other SmartX servers, the SmartX AS-B server is a Schneider Electric manufactured embedded device that generally serves as the lowest tier EcoStruxure BMS server within the EcoStruxure BMS. The SmartX server controls and supervises equipment, typically HVAC equipment. The SmartX AS-B server uses its onboard I/O with connected field devices, such as sensors and actuators, to do that.

For more information, see SmartX AS-B Servers .

MP-Cs

SmartX IP Controller – MP-C is a multi-purpose, fully programmable, IP based field controller. The MP-C models offer a flexible mix of I/O point types that suits a wide range of HVAC applications. MP-C is a native SmartX device, which can either be used as a standalone BACnet/IP field controller or as part of an EcoStruxure BMS with a SmartX AS-P or AS-B server, or an Enterprise Server, as the parent server.

For more information, see MP-Cs .

MP-Vs

SmartX IP Controller – MP-V is a multi-purpose, fully programmable, IP based field controller dedicated for VAV applications. MP-V integrates a controller, a damper actuator, and an air flow sensor in a single package for ease of installation. MP-V is a native SmartX device, which can either be used as a standalone BACnet/IP field controller or as part of an EcoStruxure BMS with a SmartX AS-P or AS-B server, or an Enterprise Server, as the parent server.

For more information, see MP-Vs .

SmartX Sensors

SmartX Sensors are a family of living space sensors designed for MP Series controllers using the EcoStruxure Building Operation user interface. These sensors use an RJ-45 sensor bus that provides communication and power from the MP Series controller.

For more information, see SmartX Sensors .

AD v1

AD v1 provides a Human Machine Interface (HMI) for local access to the EcoStruxure BMS servers.

AD v2

AD v2 is the successor to AD v1, and offers several improvements such as higher display resolution, enhanced processor performance, and increased memory size. Like AD v1, AD v2 provides a Human Machine Interface (HMI) for local access to the EcoStruxure BMS servers.

For more information, see AD v2 .

Wiring

The wiring recommendations provide guidance regarding wiring of the I/O modules, SmartX servers, and MP Series controllers.

For more information, see Wiring .

  • EcoStruxure Building Management Overview
  • Terminal Bases
  • PS-24V Power Supplies
  • Automation Servers
  • SmartX AS-P Servers
  • I/O Modules
  • SmartX AS-B Servers
  • MP-Cs
  • MP-Vs
  • SmartX Sensors
  • AD v2
  • Wiring