earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AO-8, AO-V-8, Automation Server, AS-B, DI-16, DO-FA-12, DO-FC-8, MP-C, MP-V, AS-P, PS-24V, RTD-DI-16, UI-16, UI-16 v2, UI-8/AO-4, UI-8/AO-4 v2, UI-8/AO-V-4, UI-8/AO-V-4 v2, UI-8/DO-FC-4, UI-8/DO-FC-4 v2
Functionalities: Hardware
Product version: 2.0, 2.1
6/24/2026

Status LEDs

The Status LED on the front of the SmartX devices changes color and flashes to indicate the status of the device.

 
action_zoom_plus_stroke Location of the Status LED on different SmartX device models
Figure: Location of the Status LED on different SmartX device models

The remaining LEDs on the front differ in number and meaning for the different devices and are explained in the sections about the specific device.

SmartX Server Status LED

The SmartX server Status LED indicates the condition of the device.

Table: SmartX Server Status LED Patterns

LED Patterns

Condition

Green, constant

Normal operation, status OK

Green, flashing (~1 Hz)

Device restarting, wait

Green, flashing (~10 Hz)

Device shutting down

Red, constant

Detected error, attention required

Red, flashing (~1 Hz)

Device operates, but a problem needs attention

Red/green, flashing (~1 Hz)

Device firmware upgrade (DFU) mode or firmware being downloaded in DFU mode

No light

No input power

I/O Module Status LED

The I/O module Status LED indicates the condition of the device.

Table: I/O Module Status LED Patterns

LED Patterns

Condition

Green, constant

Online and configured (at least one channel/point downloaded successfully)

Green, constant

Red, flashing (for 100 ms every 2 s)

Online and configured

Disabled Hand-Off-Auto (HOA) override switches

Applies only to I/O modules with HOA override switches and with manufacturing date earlier than 2021-W26 and upgraded with firmware version 2.017 or later. For more information, see Important Information on Central IO Modules with Manufacturing Date Earlier Than 2021-W26 .

Green, flashing (200 ms ON, 200 ms OFF)

Online and unconfigured (physical module that either matches/mismatches logical module)

Green, slow flashing (approximately every 3 s)

Low power mode (saves energy)

Red, constant

Error requiring attention (for example, the input voltage is too low)

Red, flashing (100 ms ON, 100 ms OFF)

Offline with respect to the SmartX server (both configured and unconfigured modules)

Red/Green, flashing (green 100 ms, red 100 ms)

Bootloader mode (downloading data)

No light

No input power

PS-24V Power Supply Status LED

The PS-24V power supply Status LED indicates the condition of the device.

Table: Power Supply Status LED Patterns

LED Patterns

Condition

Green, constant

Output voltage and load OK

Red/green, flashing

Output slightly overloaded

Red, constant

Output overloaded

No light

No input power

MP Series Controller Status LED

The MP Series controller Status LED indicates the condition of the device.

Table: MP Series Controller Status LED Patterns

LED Patterns

Condition

Green, constant

Normal operation, status OK

MP Series controller firmware application running

Green, flashing (~1 Hz)

Device restarting, wait

MP Series controller firmware application running

Red, constant

Detected error, attention required

Red, flashing (~1 Hz)

Device operates, but a problem needs attention

Red/green, flashing (~1 Hz)

MP Series controller I/O board receiving software upgrade, wait

Do not interrupt power to the controller. For more information, see the following Important note.

Amber, constant

MP Series controller firmware boot applet running

Amber, flash

Device restarting, wait

MP Series controller firmware boot applet started

Amber/green, flashing (~1 Hz)

MP Series controller firmware is being upgraded. It is typically the firmware main application, but it can also be a boot applet.

  • Automation Servers
  • LED Indicators
  • AS-P Servers
  • AS-P Server LEDs
  • AS-B Servers
  • AS-B Server LEDs
  • I/O Modules
  • I/O Module Operator Interface Overview
  • PS-24V Power Supplies
  • Power Supply PS-24V LEDs
  • MP-C Controllers
  • MP-V Controllers
  • MP-C Controller LEDs