The I/O modules have the following status indicator LEDs on the front of the module:
I/O Module Status LED
I/O Channel Status LEDs
Each I/O module contains a green/red Status LED that indicates the status of the I/O module in relationship to the SmartX server. The LED is labeled Status and is located on the lower right side of the I/O Module placard.
The I/O module Status LED indicates the condition of the device.
|
LED Patterns |
Condition |
|
Green, constant |
Online and configured (at least one channel/point downloaded successfully) |
|
Green, constant Red, flashing (for 100 ms every 2 s) |
Online and configured Disabled Hand-Off-Auto (HOA) override switches Applies only to I/O modules with HOA override switches and with manufacturing date earlier than 2021-W26 and upgraded with firmware version 2.017 or later. For more information, see Important Information on Central IO Modules with Manufacturing Date Earlier Than 2021-W26 . |
|
Green, flashing (200 ms ON, 200 ms OFF) |
Online and unconfigured (physical module that either matches/mismatches logical module) |
|
Green, slow flashing (approximately every 3 s) |
Low power mode (saves energy) |
|
Red, constant |
Error requiring attention (for example, the input voltage is too low) |
|
Red, flashing (100 ms ON, 100 ms OFF) |
Offline with respect to the SmartX server (both configured and unconfigured modules) |
|
Red/Green, flashing (green 100 ms, red 100 ms) |
Bootloader mode (downloading data) |
|
No light |
No input power |
Each digital input (DI) channel, digital output (DO) channel, and Universal Input (UI) channel contains a green I/O channel status LED. This LED indicates the On/Off state of the digital input or output.
You can also configure I/O channel status LEDs as an invert, so that either a HIGH or LOW voltage level can turn the LED ON.
For Universal Inputs, the I/O Channel Status LED is active only if the channel is configured as a digital input or as a counter input.