It is important to perform the grounding correctly for the following reasons:
To design a system that is not harmed by detected minor connection errors.
To design a system that works well and is resistant to EMI.
To minimize the effects of ground currents that can cause unstable measurements.
The following sections provide recommendations for designing a good working system.
This section provides grounding and power recommendations for system configurations with AS-P-3 Servers and Central IO Modules.
For more information, see Grounding and Power for Systems with AS-P-3 Servers and Central IO Modules .
This section provides grounding and power recommendations for system configurations with Central IO modules and PS-24V units.
For more information, see Grounding and Power for Systems with I/O Modules and PS-24V Units .
This section provides grounding and power recommendations for system configurations with AS-B servers.
For more information, see Grounding and Power for Systems with AS-B Servers .
This section provides grounding and power recommendations for system configurations with MP controllers.
For more information, see Grounding and Power for Systems with MP Series Controllers .
This section provides grounding and power recommendations for system configurations with IP-IO modules.
For more information, see Grounding and Power for Systems with IP-IO Modules .
This section provides grounding and power recommendations for system configurations with the RP-C controller models that support 24 VAC/VDC input power and have a half-wave rectified and non-isolated built-in power supply.
For more information, see Grounding and Power for Systems with RP-C 24 V Controller Models with Half-wave Rectified and Non-isolated Built-in Power Supply .
This section provides grounding and power recommendations for system configurations with the RP-C controller models that support 24 VAC/VDC input power and have a full-wave rectified and isolated built-in power supply.
For more information, see Grounding and Power for Systems with RP-C 24 V Controller Models with Full-wave Rectified and Isolated Built-in Power Supply .
This section provides grounding and power recommendations for system configurations with the RP-C controller models that support 230 VAC input power.
For more information, see Grounding and Power for Systems with RP-C 230 V Controller Models .
This section provides grounding and power recommendations for system configurations with the RP-C-16C-F-230V controller model and an external 24 VAC/VDC power supply connected to the EXT Input of the controller.
For more information, see Grounding and Power for Systems with RP-C-16C-F-230V-SF and External 24 VAC/VDC Power Supply .
This section provides grounding and power recommendations for system configurations with the RP-C controller models that support 230 VAC input power and RP controller expansion modules.
For more information, see Grounding and Power for Systems with RP-C 230 V Controller Models and RP Controller Expansion Modules .
This section provides grounding and power recommendations for system configurations with the RP-V controllers, which support 24 VAC input power.
For more information, see Grounding and Power for Systems with RP-V Controllers .
This section provides grounding and power recommendations for system configurations with the RP-IO I/O modules, which support 24 VAC/VDC input power and have a full-wave rectified and isolated built-in power supply.
For more information, see Grounding and Power for Systems with RP-IO Modules .
This section provides grounding and power recommendations for system configurations with Operator Display, which supports 24 VDC input power.
For more information, see Grounding and Power for Systems with Operator Display .