WebHelp is a web-based help system for the EcoStruxure Building Operation software and SmartX devices, the software and hardware that powers the EcoStruxure BMS.
By pressing F1 or clicking a Help button in the EcoStruxure Building Operation software your web browser opens WebHelp with the latest, up-to-date, technical documentation.
Some EcoStruxure Building Operation software products give you context-sensitive help by opening a WebHelp page that explains the view or dialog box you have in focus. Some programs open up an overview page. From these pages, you can follow the links to get more detailed information.
WebHelp contains all the technical information that is in the guides, specification sheets, and installation sheets.
When the computer running the EcoStruxure Building Operation software is not connected to the internet, a PDF file of the System Reference Guide is displayed instead of WebHelp. You can search the System Reference Guide in your PDF viewer.
Tip: Use your smartphone or tablet as a Wi-Fi hotspot and connect the computer to the internet to get access to the information on WebHelp.
One of the advantages with WebHelp is that you can reach Help without having the EcoStruxure Building Operation software installed on your computer. By entering the URL address help.sbo.schneider-electric.com you can access WebHelp from any computer, smartphone, or tablet connected to the internet.
The easiest way to find information on WebHelp is to search for it.
All technical information is gathered in one place, so you do not need to know which guide, specification sheet, or installation sheet the information is in.
To narrow down the search results, you can use these filters:
Product
Functionality
Information type
|
Information Type |
Description |
|
Concept |
Descriptive information about how something works, acts, and its purpose. |
|
User Interface |
Screen capture of the user interface and a table that describes each of the components of the user interface, such as properties or buttons. |
|
Troubleshooting |
Solutions to problems that may occur in your EcoStruxure BMS. |
|
Developers Reference |
Technical reference information intended for developers and support staff. |
|
Specifications |
Product features and technical specifications. |
|
How-to |
Step-by-step procedure that describes how to perform tasks. |
|
Hardware Installation |
Information about how to install the SmartX devices and technical specifications needed during the installation. |
Sometimes it is hard to know what terms are used in the technical documentation and thus hard to know what to search for. You can browse the WebHelp content using the Product or Functionality categories. From the Overview pages, you can link to more specific information. All the topics are related to one another using the See also links, so you can move quickly from one topic to another.
On WebHelp, you can see information for all released versions of the EcoStruxure Building Operation software and the SmartX devices. Use the Product version drop-down menu to jump between versions. If you are entering WebHelp from the EcoStruxure Building Operation software by pressing F1 or clicking a Help button, WebHelp automatically detects the version of the software installed and shows information for that version. Each page on WebHelp displays the versions of the product the information is valid for.
WebHelp is available to all people connected to the internet, but some information on the site is only for Schneider Electric partners and employees. To gain access to information that is privileged, you have to be logged on.
As an EcoStruxure Building Operation user, you can register an account and log on to WebHelp and subscribe to information updates.
You can rate the information on WebHelp by clicking one of the stars in the upper right corner of a topic. When you click on a star, you get the option to provide feedback on the information. If you find information you think is incorrect, you can let us know by using the rating functionality.
At the end of each page on WebHelp, you find the Community Content section. This section displays information from other employees, partners, and EcoStruxure Building Operation users. The comments are about the functionality described on the page, such as tips and additional information. You need to be logged on to be able to contribute to the Community Content.
All the information on WebHelp is also available in PDF format on the Exchange Extranet. Search for the name of the guide, specification sheet, or installation sheet. You can narrow the results by setting the Offer filter to EcoStruxure Building and the Language filter to the appropriate language.
This guide contains information on how to configure an EcoStruxure BMS, including information on protocols, devices, and external editors. The information is targeted towards Schneider Electric partners or employees who are engineering a site. This guide does not include information about hardware and WebReports with the exception of Troubleshooting and Deep Technical information.
The information in this guide is privileged information on WebHelp.
This guide contains information on how to set up features of an EcoStruxure BMS, such as user accounts and alarms. The information is targeted towards customers or Schneider Electric partners or employees who are administrating a site. This guide does not include information about hardware and WebReports.
The information in this guide is available for everyone on WebHelp.
This guide contains information how to configure WebReports and set up report features. The information is targeted towards customers or Schneider Electric partners or employees engineering and/or administrating a site.
The information in this guide is available for everyone on WebHelp.
This guide contains information on the SmartX devices, such as wiring, in/output characteristics, and RS-485 communications. The information is targeted towards Schneider Electric partners or employees and/or cabinet designers.
The information in this guide is available for everyone on WebHelp.
This guide contains information on how to administer an EcoStruxure BMS from an IT perspective, such as installation, licenses, and backups. The information is targeted towards the customers' IT departments. The information in this guide is also in the System Reference Guide or in the WebReports Reference Guide.
The information in this guide is available for everyone on WebHelp.
This guide contains information on how to upgrade an EcoStruxure BMS. The information is targeted towards Schneider Electric partners or employees upgrading a site.
The information in this guide is privileged information on WebHelp.
This guide provides information about Project Configuration Tool, such as project configuration, virtual EcoStruxure BMS server configuration, and deployment. The information is targeted towards Schneider Electric partners or employees who are engineering a site offline using Project Configuration Tool.
The information in this guide is privileged information on WebHelp.
This guide provides information about the conversion of a TAC Vista system into an EcoStruxure BMS. The information is targeted towards Schneider Electric partners or employees who are performing a conversion from a TAC Vista system using TAC Vista Conversion Tool.
The information in this guide is privileged information on WebHelp.
This guide provides information about the eCommission SmartX Controllers mobile application and its use for I/O checkout, flow balancing, and other operations aimed at commissioning and maintaining a building system that contains SmartX IP Controller devices. The information is targeted towards Schneider Electric partners or employees who are commissioning and maintaining a site using the eCommission SmartX Controllers mobile application.
The information in this guide is privileged information on WebHelp.
This guide contains information on WorkStation, such as logging on, monitoring alarms, and editing schedules. The information is targeted towards customers operating a site.
The information in this guide is available for everyone on WebHelp.
This guide contains information on WebStation, such as logging on, monitoring alarms, and editing schedules. The information is targeted towards customers operating a site.
The information in this guide is available for everyone on WebHelp.
This guide contains information on WebReports, including viewing and printing reports. The information is targeted towards customers operating a site.
The information in this guide is available for everyone on WebHelp.
This guide contains information on the eCommission SmartX Controllers mobile application, such as performing I/O checkout and other commissioning operations on SmartX IP Controller devices. The information is targeted towards electricians using the mobile application.
The information in this guide is available for everyone on WebHelp.
This guide contains information on the eCommission SmartX Controllers mobile application, such as performing flow balancing on SmartX IP Controller devices. The information is targeted towards flow balance technicians using the mobile application.
The information in this guide is available for everyone on WebHelp.
This guide describes the differences between using the Function Block Editor and the Menta Editor. The information is targeted towards Schneider Electric partners or employees who are familiar with Menta Editor. The Function Block Editor information is also available in the Technical Reference Guide.
The information in this guide is privileged information on WebHelp.
This guide describes the differences between using the Plain English Editor and the Script Editor. The information is targeted towards Schneider Electric partners or employees who are familiar with Plain English. The Script information is also available in the Technical Reference Guide.
The information in this guide is privileged information on WebHelp.
This guide contains information about important considerations that need to be taken when designing an EcoStruxure BMS, such as maximum number of devices per EcoStruxure BMS server. This guide also includes reference architectures and planning guidance for the secure deployment and configuration of an EcoStruxure BMS. The information is targeted towards Schneider Electric partners or employees who are planning a site.
The information in this guide is privileged information on WebHelp.
This guide contains information on how to provide our customers an IT-friendly and secure EcoStruxure BMS, such as port numbers and software requirements. The information is targeted towards IT professionals who need to review the system design and provide support for the system installation.
The information in this guide is privileged information on WebHelp.
Specification sheets contain information on product features and technical specifications. There is typically one specification sheet for each product:
WorkStation
WebStation
Enterprise Central
Enterprise Server
SmartX AS-P server
SmartX AS-B server
Automation Server
MP-C
MP-V
RP-C
RP-C-EXT-MS-BLE
RP-C-EXT-BL-4-HV-PD
RP-C-EXT-0-10V-4-PD
RP-C-EXT-BL-2-LV-PD
RP-C-EXT-DALI-M-PD
Engage
eCommission SmartX Controllers
AD v3
Reports Server
Project Configuration Tool
Automated Engineering Tool
Expert Tool
IP-IO
DI-16
RTD-DI-16
UI-16
AO-8 and AO-8-H
AO-V-8 and AO-V-8-H
DO-FA-12 and DO-FA-12-H
DO-FC-8 and DO-FC-8-H
UI-8/AO-4 and UI-8/AO-4-H
UI-8/AO-V-4 and UI-8/AO-V-4-H
UI-8/DO-FC-4 and UI-8/DO-FC-4-H
PS-24V
USB-485-INET
The specification sheets are available from the main menu on WebHelp.
The information in the specification sheets is available to everyone on WebHelp.
Installation sheets contain information on how to physically install our SmartX devices. These documents are shipped with the product to support the panel builder or the technician mounting the device:
AS-P
Terminal Base TP-ASP-W1
AS-B
MP-C
MP-C Display
MP-V
RP-C-12A, -12B, and -12C Models
RP-C-16A Model
RP-C-EXT-MS-BLE
RP-C-EXT-BL-2-LV-PD and RP-C-EXT-BL-4-HV-PD
RP-C-EXT-0-10V-4-PD
RP-C-EXT-DALI-M-PD
eCommission Bluetooth Adapter
AD v3
IP-IO Module
W1-Sized I/O Modules
Terminal Base TB-IO-W1
W1-Sized AS Modules
Terminal Base TB-AS-W1
W1-Sized PS Modules
Terminal Base TB-PS-W1
Xenta to AS-P Adapter
USB-485-INET
For more detailed information on the SmartX devices, refer to the SmartX Controllers Hardware Reference Guide.
The information in the installation sheets is available to everyone on WebHelp.