earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WebReports
Functionalities: Reports
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3
12/16/2021

Reporting Agent

The Reporting Agent is a Windows service that performs reads of historical data, such as extended trends, events, and alarms. During the installation, the WebReports Installer prompts you to enter the number of seconds that you want the Reporting Agent to perform these reads. It is recommended that you accept the default value.

Reporting Agent Log File

The log file for the Reporting Agent contains error, warning, debugging, and informational messages that can be used for identifying problems with the Reporting Agent.

During the installation, you set the size of the file and specify the number of log files you want to keep. The default values are recommended.

For more information, see Reporting Agent Log File .

Reporting Agent Configuration File

The Reporting Agent configuration file contains values for the following settings:

  • The Reporting Agent failure retry interval

  • The Reporting Agent log file

  • The Reporting Agent event record

  • The Reporting Agent total historical records

For more information, see Reporting Agent Configuration File .

  • WebReports Installer and WebReports Components
  • Reporting Agent Log File
  • Reporting Agent Configuration File
  • Reporting Agent does not Connect to Enterprise Server