earth_america
user_standard Log on
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: WorkStation, WebStation
Functionalities: Alarms, Basic Functionality
Product version: 7.1
4/29/2026

Temporary User Filters

You change the filter conditions to narrow what is displayed in the Alarms pane, Events pane, Alarm View, or Event View.

When you do not need to reuse the changes made to the filter conditions, you temporarily change the user filter. In this case, the changes are no longer available when you close the pane or View or log off.

If you want to save the changes made to the filter conditions, you can save the user filter as a favorite before closing the pane or View and before logging off. For more information, see Favorites .

Sorting and using fields in WebStation

You can add or remove information fields in the Alarm View and Event View in WebStation. The fields in WebStation display alarm and event information. For example, if you want to see the last comment of the alarms and who acknowledged the alarms you can add the field Last comments and Acknowledge by.

You can sort alarms and events in the Alarm View and Event View in WebStation. The sorting can be done ascending or descending. You don’t have to add the field that you sort on. For example, you can sort the alarms by priority without adding the priority field.

The sorting and adding of fields can be saved as a Favorite in WebStation. For more information, see Favorites .

Filter on a specific value

You can filter on a specific value in an alarm view in WebStation.

For more information, see Filtering on a Specific Value in an Alarm View .

  • How Alarms Work
  • How Events Work
  • Editing a User Filter
  • Editing a User Filter
  • Editing a User Filter in WebStation
  • Favorites
  • Adding a Favorites
  • Adding a Favorite in WebStation
  • Filtering on a Specific Value in an Alarm View