This following applicable documentation is useful for installing the BACnet smoke control system equipment.
Document Number |
Document Title |
F-24719-2 |
TAC I/A Series MicroNet BACnet Smoke-Control Systems Manual |
30-3001-837 |
b-Link Installation Sheet |
30-3001-1007 |
Andover Continuum UL 864 BACnet Smoke Control System Design Guide |
04-16015-0x-en |
EcoStruxure BMS Smoke Control System Enclosure Guide |
01-16001-xx-en |
EcoStruxure BMS Smoke Control System Approved Software Revisions |
04-40001-0x-en |
SpaceLogic Hardware Reference Guide |
02-18018-xx-en |
SpaceLogic AS-P-SMK and AS-P-NLS-SMK Servers Installation Sheet |
02-20041-xx-en |
SpaceLogic MP-C-SMK Controller Models Installation Sheet |
02-20045-xx-en |
SpaceLogic MP-V-SMK Controller Models Installation Sheet |
02-20046-xx-en |
SpaceLogic IP-IO-SMK I/O Module Models Installation Sheet |
When installing the model MNB-300, MNB-V1-2 or MNB-V2-2 controllers in a smoke control system, refer to the F-24719-2 manual for installation information.
When installing any of the b3 series controllers or b-Link Repeaters described in this guide, refer to the 30-3001-837 or 30-3001-1007 manuals for installation information. For more information, see MS/TP BACnet Field Controllers .
To determine the approved software revisions for the smoke control system, refer to the 01-16001-xx-en document for more information.
The SpaceLogic Hardware Reference Guide can be consulted for additional information on the PS-24V, AS-P/AS Servers, MP-C, MP-V, and IP-IO family of IP controllers, and the family of Central IO modules.
This guide takes precedence over the other manuals in regards to the system composition, configuration, architecture and restrictions/guidelines applicable to engineering the EcoStructure BMS smoke control system.