earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Alarms
Product version: 2024
10/30/2025

System Alarm ID M-NW8 R

Listed below are the System Alarms with IDs that begin with the letters M-NW8 R.

Table: System Alarms M

System Alarm ID

Description

Module type mismatch

The module type based on the user’s configuration is different from the type of the actual physical module occupying the same slot.

More than one server with the same name in the system

There is more than one EcoStruxure BMS server with the same name in the EcoStruxure BMS.

Table: System Alarms Ne-No

System Alarm ID

Description

NETWORK 8000 message

An unknown NETWORK 8000 message with specific included contents was received.

NETWORK 8000 message end

End of a NETWORK 8000 unknown message.

Network offline

The server cannot connect to the specified network.

New application program

The Xenta device has received a new valid application.

No file name set

No file name has been specified.

No valid Blueprint File

Invalid Xenta device program definition.

Not enough flash memory for log

The request was valid but could not be performed because there is not enough flash memory.

Not enough RAM memory for log

The request was valid but could not be performed because there is not enough RAM memory.

Notification files storage capacity reached

Storage capacity has been reached for notification files. For more information, see Deleting a Notification Written to a File .

  • System Alarm ID List
  • System Alarms
  • System Alarm ID A-D
  • System Alarm ID E-L
  • System Alarm ID P-S
  • System Alarm ID T-X
  • Deleting a Notification Written to a File