earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AD v1
Functionalities: Hardware
Product version: 3.3, 2022, 2023, 2024, 7.0
12/17/2021

AD v1 Communication and Power

AD v1 can use either a wired (USB) connection or a wireless (WiFi) connection to communicate with EcoStruxure BMS servers. AD v1 can be powered either by a AS-P server, AS-B server, or USB power adapter.

Communication over a USB Connection

The preinstalled AD-Link application enables AD v1 to communicate with EcoStruxure BMS servers over a USB connection.

When AD v1 is connected to a AS-P server or AS-B server, AD v1 can be powered by the automation server through the USB cable. The screen must not be turned on constantly because this may drain the battery.

Notice

LOSS OF DATA OR POWER

  • Use only USB cables ordered from Schneider Electric.

  • Use only USB cables that are designed for AD.

  • Do not use USB cables that exceed 3 m (10 ft).

Failure to follow these instructions can result in loss of data or power.

 
action_zoom_plus_stroke USB connection to a AS-P server or AS-B server
Figure: USB connection to a AS-P server or AS-B server

Communication over a Wireless Connection

AD v1 can communicate with EcoStruxure BMS servers through a wireless access point (AP), which is connected to the same network as the EcoStruxure BMS servers. When used as a stationary HMI terminal, AD v1 is connected to a USB power adapter to ensure that its battery is charged.

Warning Warning

HAZARD OF EXPLOSION OR DEVICE DAMAGE

Use only Samsung-approved power adapters.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

 
action_zoom_plus_stroke Wireless communication and power from a USB power adapter
Figure: Wireless communication and power from a USB power adapter
  • AD v1
  • Hardware Overview
  • Connecting an Advanced Display to an AS-P server or AS-B server
  • Connecting Advanced Display to a Power Adapter