AD v2 uses a wired (USB) connection to communicate with EcoStruxure BMS servers. During installation and commissioning, you can use a wireless access point to establish communication between AD v2 and EcoStruxure BMS servers. AD v2 can be powered either by a SmartX AS-P server, SmartX AS-B server, or USB power adapter, but not by an Automation Server.
Communication over a USB Connection
The preinstalled SmartX AD-Link application enables AD v2 to communicate with EcoStruxure BMS servers over a USB connection.
When AD v2 is connected to a SmartX AS-P server or SmartX AS-B server, AD v2 can be powered by the SmartX server through the USB cable. The screen must not be turned on constantly because this may drain the battery.
action_zoom_plus_stroke
USB connection to a SmartX AS-P server or SmartX AS-B server
Notice
|
LOSS OF DATA OR POWER
Use only USB cables ordered from Schneider Electric.
Use only USB cables that are designed for AD.
Do not use USB cables that exceed 3 m (10 ft).
Failure to follow these instructions can result in loss of data or power.
|
When AD v2 is connected to an Automation Server, AD v2 must be powered by a USB power adapter. The Automation Server does not provide enough power for AD v2. A USB “Y” cable allows you to connect AD v2 to two different devices, an Automation Server and a USB power adapter, to receive data and power respectively. The screen must not be turned on constantly because this may drain the battery.
action_zoom_plus_stroke
USB connection to an Automation Server and a USB power adapter
Use only Samsung-approved power adapters. Using other power adapters can cause the battery to explode or damage the tablet.
Warning
|
HAZARD OF EXPLOSION OR DEVICE DAMAGE
Use only Samsung-approved power adapters.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
|