earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: AS-B, Edge Server, Enterprise Central, Enterprise Server, AS-P, Virtual Project Servers
Functionalities: Engineering
Product version: 2023
2/11/2026

Default System Folder

You use the default System folder for a number of engineering operations in your EcoStruxure BMS.

 
action_zoom_plus_stroke Default System folder
Figure: Default System folder

Table: Default System Folder

Item

Description

Alarm Control Panel

Use Alarm Control Panel to manage overrides of alarm configurations, actions required when alarms are triggered, and the appearance of alarms in different alarm states.

For more information, see Alarm Decoration .

For more information, see User Actions .

For more information, see Alarm Styles View .

Backup and Restore

Use the Backup and Restore folder to manage backup rules, backup set, and to open Backup and Restore Manager for Enterprise Server and Enterprise Central to supervise the backup settings in the EcoStruxure BMS.

For more information, see Backup Rules .

For more information, see Backup Sets .

For more information, see Backup and Restore Manager on the Enterprise Server .

Binding Templates

Use Binding Templates to add and view binding templates in the Building Operation EcoStruxure BMS.

For more information, see Binding Templates .

Connect Settings

Use Connect Settings to enable the transfer of system information and crash information of the EcoStruxure BMS servers to the Connect storage server.

For more information, see Connect Agent Overview .

Content Types

Use Content Types to view the folders and container objects that use a content type.

For more information, see Content Types .

Domains

Use Domains to add and view domains in the EcoStruxure BMS.

For more information, see Domains .

EcoStruxure Web Services

Use EcoStruxure Web Services to configure how information in XML format is translated so that it can be understood by EcoStruxure BMS servers and displayed in WorkStation.

For more information, see Web Services .

Firmware

Use Firmware to save MPx firmware on the server.

Hardware

Use Hardware to view the hardware included in the EcoStruxure BMS.

Interface Manager

Use the Interface Manager to view the priority levels based on the BACnet standard and set the COV subscription frequency and renewal rate on a lead EcoStruxure BMS server for the BACnet system.

For more information, see Interface Manager for BACnet – Basic Tab .

LonWorks Binding Profile

Use LonWorks Binding Profiles to view binding profiles that determine the behavior of LonWorks bindings.

For more information, see LonWorks Binding Profiles .

Modules

For more information, see Central IO Modules Overview .

Notification Files

Use Notification Reports to view files containing important information on the EcoStruxure BMS.

For more information, see Notification Reports .

Ports

Report Manager

User Report Manager to configure certain parameters required to generate, view, and create reports in WorkStation.

SmartDrivers

Use SmartDrivers to add customized interfaces in the EcoStruxure BMS that monitors and controls third-party devices from an EcoStruxure BMS server.

For more information, see SmartDrivers Overview .

Tasks

Use Tasks to connect Function block and Script programs to tasks.

For more information, see Tasks .

Time Settings

Use Time Settings to configure EcoStruxure BMS server time settings and time zone setting.

For more information, see Automation Server – Date & Time View .

Archive Settings

Use Archive Settings to configure how data from selected events and extended trend logs is to be preserved.

For more information, see Archiving Overview .

Bindings Diagnostics

Use Bindings Diagnostics to check the database for unresolved or invalid references.

For more information, see Bindings Diagnostics .

Security Manager

Use System Manager configure features that help you increase the security in your EcoStruxure BMS.

For more information, see Security Overview .

Server Communicatio n

Use Server Communication to view the communication settings of the server. For more information, see EcoStruxure BMS Server Communication .

SystemControlPanel

Use Control Panel to access some of the most used functions in the EcoStruxure BMS.

For more information, see Control Panel Tab .

  • EcoStruxure Building Operation Objects
  • Alarm Decoration
  • User Actions
  • Alarm Styles View
  • Backup Rules
  • Backup Sets
  • Backup and Restore Manager on the Enterprise Server
  • Binding Templates
  • Connect Agent Overview
  • Content Types
  • Domains
  • Web Services
  • Hardware Overview
  • Interface Manager for BACnet – Basic Tab
  • LonWorks Binding Profiles
  • Central IO Modules Overview
  • Notification Reports
  • Progress View
  • SmartDrivers Overview
  • Tasks
  • Automation Server – Date & Time View
  • Archiving Overview
  • Bindings Diagnostics
  • Security Overview
  • EcoStruxure BMS Server Communication
  • Control Panel Tab