Use the Time and Date editor to configure the network time server addresses or configure time on EcoStruxure BMS servers.
|
Property |
Description |
|
Use external NTP server |
Select Enabled to define the primary and secondary NTP server addresses for connected shadow EcoStruxure BMS server devices. |
|
NTP Server 1 |
Type the address to the primary time server to which the shadow SmartX server date and time object synchronizes its clock. |
|
NTP Server 2 |
Type the address to the secondary time server to which the shadow SmartX servers' date and time object synchronizes its clock. |
|
Lead object |
Enter the object that acts as the lead for this object. |
|
NTP Server 1 Key Id |
Type the ID of the authentication key for the primary time server. |
|
NTP Server 2 Key Id |
Type the ID of the authentication key for the secondary time server. |
|
NTP Server 1 Key Value |
Type the password for the primary time server. |
|
NTP Server 2 Key Value |
Type the password for the secondary time server. |
|
Authenticate Network Time Synchronization |
Select if you want to use authenticated network time synchronizing. |
|
Date and time |
Configure the date and time if you do not want to use an external NTP server. |