earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: IP-IO , MP-C
Functionalities: Hardware
Product version: 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0
11/1/2023

Home Screen on MP-C or IP-IO Module

Use the Home screen to get information on the MP-C or IP-IO module model name, BACnet ID, and TCP/IP configuration settings.

 
action_zoom_plus_stroke Home screen on MP-C or IP-IO module
Figure: Home screen on MP-C or IP-IO module

Table: Home screen on MP-C or IP-IO module

Component

Description

[Model name]

Displays the MP-C or IP-IO module model name.

BACnet ID: [BACnet ID]

Displays the MP-C or IP-IO module BACnet ID.

IP Assign: [Assignment method]

Displays the IP address assignment method used for assigning an IP address to the MP-C or IP-IO module. For more information, see IP Address Assignment for SmartX IP Controllers .

IP: [IP address]

Displays the MP-C or IP-IO module IP address.

SM: [Subnet mask]

Displays the subnet mask, which is used to determine what subnet the MP-C or IP-IO module belongs to.

GW: [Default gateway]

Displays the default gateway (router) address.

MAC: [MAC address]

Displays the MP-C or IP-IO module MAC address.

  • Output Override Function
  • User Experience
  • IP Address Assignment for SmartX IP Controllers