You use the SpaceLogic Sensor 
Display
 property tabs in WorkStation to view and configure the UI features of the various sensor models within your control application.
 The Display 
Basic
 tab properties includes the same 
General Information
 you find on all EcoStruxure Building Operation objects. Beyond that, it also provides a 
Setpoint
, a 
Fan speed
, an 
Occupancy override
, an 
HVAC mode
, a 
Heating cooling status
, and 4 
Custom value text
 fields. In addition, there are several properties that allow you to control the temperature display. For example, the 
Temperature display mode
 allows you to configure the temperature value displayed on the SpaceLogic Sensor display in its passive display state with the following settings:
- 
Live Temperature
: Displays the space temperature measured by the SpaceLogic sensors internal temperature sensor
 
- 
Temperature setpoint
: Displays the current setpoint temperature value
 
- 
Custom temperature
: Displays the value of the Custom temperature property
 
The Custom temperature property then allows you to display any value in the temperature range, either by referencing another temperature source (for example, an external temperature sensor) or by setting it manually in the Custom temperature field (warm start retained only).
  Advanced Tab
The Display 
Advanced 
property tab includes considerably more configuration information. For example, you turn on the 
Allow menu page
 property to display all submenus including the Functions menu and any of its submenus. Should you wish, you can enable the temperature setpoint feature by setting the Display object 
Allow setpoint changes
 property to 
On
 and configuring the 
Setpoint high limit
 and 
Setpoint low limit
 properties. If colored wall back lighting feedback is required for the room occupant, you can turn on the 
Enable wall back lighting
 property. 
  
        Note:
    
Allow setpoint changes, Setpoint high limit, and Setpoint low limit are the types of properties you may wish to drive dynamically based on time of day. For example, using a schedule, you may only allow setpoint changes during the day and not at night. You may also only change the high and low limits for the setpoint based on whether you are in the heating or cooling season. 
   
 
In addition, you can use the 
Occupancy override icon
 property and its 
Command
 and 
State
 options as follows: 
- 
Command
: When occupied, the house is empty. When clicked, the Command to vacate or unoccupy is sent.
 - 
When unoccupied, the house displays with a person inside. When clicked, the Command to occupy is sent.
 
- 
State
: When the house displays with a person inside, it indicates the current state is occupied. When clicked, the State command to unoccupy is sent.
 - 
When unoccupied, the house is empty to indicate its current state. When clicked, the State command to occupy is sent.
 
Finally, you can enable lighting and blind control functions using the Display object 
Allow light control
 and 
Allow blind control 
properties. Within the light function, you can toggle on and off or set a percentage to control the intensity of the lights using the 
Lighting mode
 property. Similarly, you can you can toggle on and off or set a percentage to control the blind louver sub-function using the 
Blind control mode
 property. 
  Light and Blind Control Tab
For more granular control, you can use the Light and Blind Control tab to specify the 4 supported light groups, and the blind position and angle for the 12 supported blind groups in the SpaceLogic Sensor. You can also use the 
Light forced disable
 and 
Blind forced disable
 properties as an override or a forced disable.
  Light and Blind Configuration Tab
In this tab, you can enter the 
Default light group
 or 
Default blind group
 value corresponding to the Light and Blind Control tab 
Light 1-4 level 
and 
Blind 1-12 position 
properties. For example, if you select Default light group or Default blind group equals 1, you direct the Remote Control to affect the Light 1 level and the Blind 1 angle and Blind 1 position properties.
  Button and Scene Configuration Tab
The Display 
Button and Scene Configuration 
property tab allows you to select from the available functions or scenes to program the buttons on the SpaceLogic Sensor display models. You can also select the buttons you wish to display for configured scenes and triggers for each of the scene buttons. 
For more information, see Configuring SpaceLogic Sensor Display Properties
.
    
        
    
        Property Mapping
    
        
While the Display property tabs allow you to configure varied SpaceLogic Sensor models with different UI features, not all of the properties apply to each model. Be sure to consider this when configuring the application and binding it to your control programs. The table that follows shows the properties applicable to each unit. 
 
    
Table: SpaceLogic Sensor and Display Object Property Mapping
| 
Display property
 | 
Touchscreen Display
 | 
LCD Temperature Sensor
 | 
 3-Button Cover
 | 
| 
Setpoint 
 | 
Yes
 | 
Yes
 | 
Yes
 | 
| 
Fan speed
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Occupancy override
 | 
Yes
 | 
Yes
 | 
Yes
 | 
| 
HVAC mode
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Selected scene
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Light level
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Blind position
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Blind slat angle
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Temperature display mode
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Custom temperature
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Heating cooling status
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Show time
 | 
Yes
 | 
No
 | 
No
 | 
| 
Time format
 | 
Yes
 | 
No
 | 
No
 | 
| 
Show CO2
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Show humidity
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Temperature units
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Allowed fan speeds
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Enable wall back lighting
 | 
No
 | 
No
 | 
Yes
 | 
| 
Lighting mode
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Blind control mode
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Blind angle mode
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Allowed HVAC modes
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Allow setpoint changes
 | 
Yes
 | 
Yes
 | 
Yes
 | 
| 
Setpoint high limit
 | 
Yes
 | 
Yes
 | 
Yes
 | 
| 
Setpoint low limit
 | 
Yes
 | 
Yes
 | 
Yes
 | 
| 
Allow fan speed changes
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Allow occupancy overrides
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Allow HVAC mode changes
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Allow menu pages
 | 
Yes
 | 
No
 | 
No
 | 
| 
Allow sensors information pages
 | 
Yes
 | 
No
 | 
No
 | 
| 
Allow device information page
 | 
Yes
 | 
No
 | 
No
 | 
| 
Allow parent information page
 | 
Yes
 | 
No
 | 
No
 | 
| 
Allow custom information page
 | 
Yes
 | 
No
 | 
No
 | 
| 
Allow temperature unit changes
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Allow light control
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Allow blind control 
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Display backlight
 | 
Yes
 | 
No
 | 
No
 | 
| 
Button (1-12) function
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Scene button (1-8) button
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
Scene button (1-8) trigger
 | 
Yes
 | 
Yes
 | 
No
 | 
| 
SpaceLogic Living Space Sensor / Eco mode
 | 
Yes
 | 
Yes
 | 
Yes
 |