earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
Concept

Concept


Products: SpaceLogic Sensor
Functionalities: Hardware, Touchscreen
Product version: 2.0, 2.1, 3.0
6/6/2019

SmartX Sensor Touchscreen Display Model

arrow1_rotationDisplay Object arrow1_rotationScript Program Property Configuration arrow1_rotationInformation Pages

The Touchscreen Display model provides a menu-driven interface with a main menu and an optional default or home screen configurable through EcoStruxure Building Operation.

Using these screens, you can perform a variety of tasks including:

 
action_zoom_plus_stroke SmartX Sensor touchscreen display model

SmartX Sensor touchscreen display model

Display Object

The vast majority of the properties in the Basic and Advanced tabs of the Display object are valid for the SmartX Sensor Touchscreen Display model, including the setpoint, fan speed, occupancy override and HVAC mode. For example, you can turn the time off on the Advanced page using the Show time property. Once you save your choice, you can watch the time disappear on the display. Similarly, you can switch from the 12-hour to the 24-hour format using the Time format property. You can also turn off CO2 and humidity on the display’s default screen. For more information, see SmartX Sensor Touchscreen Display Model- Default Screen .

You can configure your specific fan type depending on the type of fan located in your zone. Typically, you only need to set this once because the zone equipment either does, or does not include a fan. If it does, it only has so many speeds, further limiting the available choices.

For more information, see Configuring the Fan Speed .

You can use the available options to configure the Display back light property. For example, you can turn the light On by motion since it includes a motion sensor, or you can configure it to turn On by touch , so that when someone touches it, it wakes up and turns on. This is a property you may just configure once or perhaps configure it based on the time of day since you may not want the back light turning on at night.

Note:

There is no wall back lighting for the SmartX Sensor Touchscreen Display mode, so the Enable wall back lighting property is not supported here.

Script Program Property Configuration

You can bind to the Display object properties and read them into your Script programs. There are also properties that you might want to configure from your Script programs. For instance, you can drive the heating and cooling status indicator to show that you are actively heating or cooling and also animate the background color of the display. Specifically, you may display a pink background when actively heating and a blue background when actively cooling. Similarly, you may want to drive the fan speed to show whether your program has overridden the fan speed and if this is no longer what the user specified.

It can be difficult to drive a property from a program since reading and writing to a program simultaneously can be challenging without overwriting objects. Be aware that there is a a technique for waiting and then writing a null back so you do not overwrite your objects.

Information Pages

A unique feature in the SmartX Sensor Touchscreen Display model are the information pages which allows users access to information about the on-board sensors, the sensor device itself, the parent MP Series controller, and custom text messages. You access information pages by clicking the information icon

 
action_zoom_plus_stroke
at the top of the main menu which is enabled using the Display object Allow menu page property. If the icon is not visible, the Allow sensors information page , Allow device information page , Allow parent information page , and Allow custom information page properties in the Display object are turned off. You are not permitted to access the information pages.

Important:

System administrators or control system engineers may wish to turn off access to some these pages after the commissioning phase of a project to prevent exposing internal data like Device IDs and IP addresses to room occupants. There may be a perceived Cybersecurity risk with exposing this information after the building has been commisionned and turned over. It may also be sensitive information that system admins and control engineers may not want in user’s hands. As a result, they should evaluate the information on these pages when the job is initially configured to decide whether it should be exposed.

  • SmartX Sensor Models
  • Changing the Temperature Setpoint
  • Configuring the Fan Speed
  • Configuring the Degree Type
  • Changing the Occupancy Mode
  • Changing the HVAC Mode