SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen
Use the SpaceLogic Sensor LCD Temperature Sensor model Default screen to advance through the menus, increase and decrease temperature, change modes and degree types, and perform occupany overrides.
action_zoom_plus_stroke
Figure:
SpaceLogic Sensor LCD Temperature Sensor model- default screen
Table: SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen
Button
|
Description
|
action_zoom_plus_stroke
|
Press to decrease the temperature.
Press to toggle backwards through menu items, such as heating and cooling and occupany modes.
|
action_zoom_plus_stroke
|
Press to advance from the default menu through items for heating and cooling and occupancy, and changing humidity, and Celsius and Fahrenheit degree types.
|
action_zoom_plus_stroke
|
Press to increase the temperature.
Press to change the fan speed.
Press to toggle between heating and cooling and occupied and unoccupied modes.
|
SpaceLogic Sensor 3-Button Cover Model
SpaceLogic Sensor LCD Temperature Sensor Model- Home Screen
SpaceLogic Sensor LCD Temperature Sensor Model- Fan Speed Screen
SpaceLogic Sensor LCD Temperature Sensor Model- Heating and Cooling Mode Screen
SpaceLogic Sensor LCD Temperature Sensor Model- Degree Type Screen
SpaceLogic Sensor LCD Temperature Sensor Model- Occupancy Mode Screen
Changing the Temperature Setpoint
Changing the Fan Speed
Changing Heating and Cooling Mode Settings
Changing the Occupancy Mode
Changing the Degree Type