earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: SpaceLogic Sensors
Functionalities: Hardware, LCD
Product version: 3.3, 2022, 2023, 2024
7/23/2021

SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen

Use the SpaceLogic Sensor LCD Temperature Sensor model Default screen to advance through the menus, increase and decrease temperature, change modes and degree types, and perform occupany overrides.

 
action_zoom_plus_stroke SpaceLogic Sensor LCD Temperature Sensor model- default screen

SpaceLogic Sensor LCD Temperature Sensor model- default screen

Table: SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen

Button

Description

 
action_zoom_plus_stroke

Press to decrease the temperature.

Press to toggle backwards through menu items, such as heating and cooling and occupany modes.

 
action_zoom_plus_stroke

Press to advance from the default menu through items for heating and cooling and occupancy, and changing humidity, and Celsius and Fahrenheit degree types.

 
action_zoom_plus_stroke

Press to increase the temperature.

Press to change the fan speed.

Press to toggle between heating and cooling and occupied and unoccupied modes.

  • SpaceLogic Sensor 3-Button Cover Model
  • SpaceLogic Sensor LCD Temperature Sensor Model- Home Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Fan Speed Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Heating and Cooling Mode Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Degree Type Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Occupancy Mode Screen
  • Changing the Temperature Setpoint
  • Changing the Fan Speed
  • Changing Heating and Cooling Mode Settings
  • Changing the Occupancy Mode
  • Changing the Degree Type