Use this workflow to connect the eCommission SmartX Controllers mobile application to SmartX IP controllers.
Related information can be found in the sections that follow the flowchart.
Download, install, and activate the eCommission application, and accept the end user license agreement.
For more information, see Downloading and Starting the eCommission SmartX Controllers Mobile Application .
For more information, see Launching and Activating the eCommission SmartX Controllers Mobile Application .
Power up the SmartX IP controllers.
For more information, see Powering Up MP-C .
For more information, see Powering Up MP-V .
Prepare a wired or wireless connection for use with the eCommission application mobile device.
|
Connection Type |
More Information |
|
Wired connection to a single controller |
For more information, see Connecting to Single SmartX IP Controller by Wire . |
|
Wired connection to a network of controllers |
For more information, see Connecting to Network of SmartX IP Controllers by Wire . |
|
Wireless connection to a network of controllers via a WiFi router |
For more information, see Connecting to Network of SmartX IP Controllers through WiFi Router . |
|
Wireless connection to a network of controllers via a wireless access point |
For more information, see Connecting to Network of SmartX IP Controllers through a Wireless Access Point . |
Start the eCommission application and then discover the SmartX IP controllers on the network.
For more information, see Downloading and Starting the eCommission SmartX Controllers Mobile Application .