earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: SpaceLogic Sensor
Functionalities: Hardware, LCD
Product version: 3.3, 2022, 2023
7/23/2021

SpaceLogic Sensor LCD Temperature Sensor Model- Fan Speed Screen

Use the SpaceLogic Sensor LCD Temperature Sensor model Fan Speed screen to view and configure the current fan speed.

 
action_zoom_plus_stroke SpaceLogic Sensor LCD Temperature Sensor Model - fan speed screen

SpaceLogic Sensor LCD Temperature Sensor Model - fan speed screen

Table: SpaceLogic Sensor LCD Temperature Sensor Model- Fan Speed Screen

Component

Description

 
action_zoom_plus_stroke

Identifies the screen as the fan speed screen.

Fan speed setting

Displays the current fan speed:

  • Off

  • 1: Low speed

  • 2: Medium speed

  • 3: High speed

  • 4: Automatic. Indicates that the fan turns on automatically ONLY when the system is heating or cooling the air.

You can change the fan speed by using the interface buttons.

For more information, see SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen .

For more information, see Changing the Fan Speed .

  • SpaceLogic Sensor LCD Temperature Sensor Model
  • SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Home Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Heating and Cooling Mode Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Fan Speed Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Degree Type Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Occupancy Mode Screen
  • Changing the Temperature Setpoint
  • Changing the Fan Speed
  • Changing Heating and Cooling Mode Settings
  • Changing the Occupancy Mode
  • Changing the Degree Type