earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: SpaceLogic Sensors
Functionalities: Hardware, LCD
Product version: 3.3, 2022, 2023, 2024
7/23/2021

SpaceLogic Sensor LCD Temperature Sensor Model- Heating and Cooling Mode Screen

Use the SpaceLogic Sensor LCD Temperature Sensor model Heating and Cooling Mode screen to view and configure the current heating or cooling setting.

 
action_zoom_plus_stroke SpaceLogic Sensor LCD Temperature Sensor Model - heating and cooling mode screen
Figure: SpaceLogic Sensor LCD Temperature Sensor Model - heating and cooling mode screen

Table: SpaceLogic Sensor LCD Temperature Sensor Model- Heating and Cooling Mode Screen

Component

Description

 
action_zoom_plus_stroke

Identifies the screen as the heating and cooling mode screen.

Heating and cooling mode setting

Displays whether heating or cooling mode is in operation:

  • H: Heating

  • C: Cooling

  • A: Automatic. Indicates that heating or air conditioning turns on automatically ONLY when the system is heating or cooling the air.

You can change heating and cooling mode settings using the interface buttons.

For more information, see SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen .

For more information, see Changing Heating and Cooling Mode Settings .

  • SpaceLogic Sensor LCD Temperature Sensor Model
  • SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Home Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Fan Speed Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Degree Type Screen
  • SpaceLogic Sensor LCD Temperature Sensor Model- Occupancy Mode Screen
  • Changing the Temperature Setpoint
  • Changing the Fan Speed
  • Changing Heating and Cooling Mode Settings
  • Changing the Occupancy Mode
  • Changing the Degree Type