SpaceLogic Sensor LCD Temperature Sensor Model- Degree Type Screen
Use the SpaceLogic Sensor LCD Temperature Sensor model Degree Type screen to view and configure the degree type setting.
action_zoom_plus_stroke
Figure:
SpaceLogic Sensor LCD Temperature Sensor Model - degree type screen
Table: SpaceLogic Sensor LCD Temperature Sensor Model- Degree Type Screen
|
Component
|
Description
|
action_zoom_plus_stroke
|
Idenfies the screen as the degree type screen.
|
|
Degree type setting
|
Displays the current degree type setting:
You can change the degree type to view the temperature in the desired unit using the interface buttons.
For more information, see SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen
.
For more information, see Changing the Degree Type
.
|
SpaceLogic Sensor LCD Temperature Sensor Model
SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen
SpaceLogic Sensor LCD Temperature Sensor Model- Home Screen
SpaceLogic Sensor LCD Temperature Sensor Model- Fan Speed Screen
SpaceLogic Sensor LCD Temperature Sensor Model- Heating and Cooling Mode Screen
SpaceLogic Sensor LCD Temperature Sensor Model- Occupancy Mode Screen
Changing the Temperature Setpoint
Changing the Fan Speed
Changing Heating and Cooling Mode Settings
Changing the Occupancy Mode
Changing the Degree Type