SpaceLogic Sensor LCD Temperature Sensor Model- Occupancy Mode Screen
Use the SpaceLogic Sensor LCD Temperature Sensor model Occupancy mode screen to view and configure the room occupancy mode.
action_zoom_plus_stroke
SpaceLogic Sensor LCD Temperature Sensor Model - occupancy mode screen
Table: SpaceLogic Sensor LCD Temperature Sensor Model- Occupancy Mode Screen
Component
|
Description
|
action_zoom_plus_stroke
|
Identifies the screen as the occupancy mode screen.
|
Occupancy mode setting
|
Displays the curent setting indicating whether the room is occupied or unoccupied:
Yes: Occupied
No: Unoccupied
You can change the occupancy mode setting to tell the control system that the room is occupied or unoccupied using the interface buttons.
For more information, see SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen
.
For more information, see Changing the Degree Type
.
|
SpaceLogic Sensor LCD Temperature Sensor Model
SpaceLogic Sensor LCD Temperature Sensor Model- Default Screen
SpaceLogic Sensor LCD Temperature Sensor Model- Home Screen
SpaceLogic Sensor LCD Temperature Sensor Model- Fan Speed Screen
SpaceLogic Sensor LCD Temperature Sensor Model- Heating and Cooling Mode Screen
SpaceLogic Sensor LCD Temperature Sensor Model- Degree Type Screen
Changing the Temperature Setpoint
Changing the Fan Speed
Changing Heating and Cooling Mode Settings
Changing the Occupancy Mode
Changing the Degree Type