Use the Entitlements Product Licenses View to view field server licenses.
|
Component |
Description |
|
Add entitlement |
Click to add an Entitlement. For more information, see Centralized Licensing Overview . |
|
Add demo license |
Click to add a demo license. For more information, see Centralized Licensing Overview . |
|
Refresh all |
Click to refresh the list. |
|
Product name |
Displays the product name of the product that contains the licenses in the row for the product. |
|
Activation ID |
Displays the activation ID. The activation ID is unique for the product and cannot be changed. |
|
[ License column] |
Displays the features that need licenses. For more information, see Software and Features that Require Licenses . |
|
Total |
Displays the total number of licenses for the product in this Entitlement. The column Total represents how many activations that are possible. Total is equivalent to the term Seats in Flexera license framework. Total does not show how many specific licenses are available. The license quantity is displayed under the corresponding license feature column. For example, if Total is set to 10 and the quantity under the license feature is 5, this means that every time you activate 1 Seat you get 5 licenses activated at once. If you choose to activate all Seats on the same server then you get 10 x 5 = 50 licenses. |
|
Available |
Displays the product's available number of licenses for the product that are not activated. |