earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
0
User Interface

User Interface


Products: AS-B, Edge Server, Device Administrator, AS-P
Functionalities: License Management
Product version: 2024
10/30/2025

Activate Licenses Offline Dialog Box

Use the Activate Licenses Offline dialog box to activate licenses on one or many field servers that are not connected to the Internet.

 
action_zoom_plus_stroke Activate Licenses Offline dialog box
Figure: Activate Licenses Offline dialog box

Table: Activate Licenses Offline Dialog Box

Component

Description

1. Create request files

Click to create request files with information on the licenses you want to activate.

For more information, see Field Server Licensing on Field Servers not Connected to Internet Workflow .

2. Activate request files on License Activation Server (FNO) to receive response files

Click to activate the request files on License Activation Server (FNO) to receive response files.

For more information, see Field Server Licensing on Field Servers not Connected to Internet Workflow .

3. Send response files to the selected automation servers

Click to send the response files with the activated licenses to the automation servers to complete the activation process.

For more information, see Field Server Licensing on Field Servers not Connected to Internet Workflow .

  • Field Server Licensing Overview
  • Field Server Licensing on Field Servers not Connected to Internet Workflow