The feature strings are used when you troubleshoot a license problem. To see the strings, you need to log on to the field server using WorkStation. The strings are visible under licensemetadata in the System tree.
Product license |
Feature string 1 |
Description |
SmartDriver |
smartdriver.license |
Use this license to allow SmartDrivers. |
SNMP Notifications |
server.alarms.snmp |
Use this license to allow SNMP notifications. |
Personal Dashboards |
client.dashboard |
Use this license to allow Personal Dashboards. |
Cloud Connectivity |
server.cloud.customer |
Use this license to allow the server to connect to the cloud using Cloud Connectivity. |
MQTT |
server.mqtt.r.w |
Use this license to allow an MQTT client to read and write to an MQTT broker. |